:FUNCtion:PARameters:DFEQualizer:PROPtimize:LTMagnitudes

Command Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:LTMagnitudes {ON | OFF}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DFEQualizer:PROPtimize:LTMagnitudes?

Description

Turns tap magnitude limits ON or OFF. When tap magnitude limits are ON, use the:FUNCtion:PARameters:DFEQualizer:PROPtimize:BMAX command to enter maximum the tap magnitude (bmax(n)) for each tap.

When tap magnitude limits are OFF, use the :FUNCtion:PARameters:DFEQualizer:PROPtimize:BMAX command to enter maximum tap values (bbmax(n)) for each tap and the :FUNCtion:PARameters:DFEQualizer:PROPtimize:BMIN command to enter minimum tap values (bbmin(n)) for each tap.

Pulse response optimization (:FUNCtion:PARameters:DFEQualizer:PROPtimize) must be on to use this command.

Automatic taps (:FUNCtion:PARameters:DFEQualizer:TAPS:AUTO) can be on or off when using this command.