:MEASure:THReshold:EREFerence
Command Syntax
:MEASure:THReshold:EREFerence {TBASe | OZERo}
Query Syntax
:MEASure:THReshold:EREFerence?
Description
Sets the reference used to when establishing custom threshold definitions.
- TBASe
- Selects custom levels based on Vtop (100%) and Vbase (0%). When
TBASeis selected, use the:MEASure:TBASe:GENeral:METHodcommand if you want to define custom the top and base levels. - OZERo
- Selects custom levels based on one and zero levels.
Example Command Sequence
:MEASure:THReshold:EREFerence OZERo