:MEASure:THReshold:GENeral:LOWer

Command Syntax

:MEASure:THReshold:GENeral:LOWer  <amplitude>

<amplitude> is a double.

Query Syntax

:MEASure:THReshold:GENeral:LOWer?

Description

Sets or queries the General threshold's global lower threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :MEASure:THReshold:GENeral:PLOWer command.

Use the :MEASure:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.

Use the :MEASure:THReshold:GENeral:UPPer command to enter a upper threshold level. Use the :MEASure:THReshold:GENeral:MIDDle command to enter a middle threshold level.

Example Command Sequence

:MEASure:THReshold:GENeral:METHod ABSolute
:MEASure:THReshold:GENeral:UPPer 125E-3
:MEASure:THReshold:GENeral:MIDDle 0E0
:MEASure:THReshold:GENeral:LOWer -125E-3