:MEASure:THReshold:PAM:RFALl:PAMLevel:LEVel{N}

Command Syntax

:MEASure:THReshold:PAM{3|4}:RFALl:PAMLevel:LEVel{N}  <amplitude>

Where {N} is the PAM level. For example, in PAM4, you can use LEVel0, LEVel1, LEVel2, or LEVel3.

<amplitude> is a double.

Query Syntax

:MEASure:THReshold:PAM{3|4}:RFALl:PAMLevel:LEVel{N}?

Description

For the PAM Rise/Fall global threshold, when the ABSolute method for PAM level definition is selected (see :MEASure:THReshold:PAM:RFALl:LMEThod), this command is used to specify the PAM level values.