:MEASure:THReshold:GENeral:PMIDdle
Command Syntax
:MEASure:THReshold:GENeral:PMIDdle <percent>
Where <percent> is a decimal number from -25.0 to +125.0.
Query Syntax
:MEASure:THReshold:GENeral:PMIDdle?
Description
When the global threshold method is a custom PERCent between top and base (see :MEASure:THReshold:GENeral:METHod), the :MEASure:THReshold:GENeral:PMIDdle command sets or queries the custom middle percent value.
Example Command Sequence
:MEASure:THReshold:GENeral:METHod PERCent :MEASure:THReshold:GENeral:PUPPer 125E-3 :MEASure:THReshold:GENeral:PMIDdle 0E0 :MEASure:THReshold:GENeral:PLOWer -125E-3