:MEASure:THReshold:PAM:GENeral:HYSTeresis
Command Syntax
:MEASure:THReshold:PAM{3|4}:GENeral:HYSTeresis <plus_or_minus_value>
<plus_or_minus_value> is a double.
Query Syntax
:MEASure:THReshold:PAM{3|4}:GENeral:HYSTeresis?
Description
For the PAM General global threshold, when the :MEASure:THReshold:PAM:GENeral:METHod setting is HYSTeresis, this command sets the ±hysteresis value.