:MEASure:THReshold:RFALl:PLOWer
Command Syntax
:MEASure:THReshold:RFALl:PLOWer <percent>
<percent> is a decimal number from -25.0 to +125.0.
Query Syntax
:MEASure:THReshold:RFALl:PLOWer?
Description
When the Rise/Fall threshold's global threshold method is a custom PERCent between top and base (see :MEASure:THReshold:RFALl:METHod), the :MEASure:THReshold:RFALl:PLOWer command sets or queries the custom lower percent value.
Example Command Sequence
:MEASure:THReshold:RFALl:METHod PERCent :MEASure:THReshold:RFALl:PUPPer 125E-3 :MEASure:THReshold:RFALl:PLOWer -125E-3