:MEASure:THReshold:PAM:GENeral:PAMLevel:LEVel{N}
Command Syntax
:MEASure:THReshold:PAM{3|4}:GENeral:PAMLevel:LEVel{N} <amplitude>
Where {N} is the PAM level. For example, in PAM4, you can use LEVel0, LEVel1, LEVel2, or LEVel3.
<amplitude> is a double.
Query Syntax
:MEASure:THReshold:PAM{3|4}:GENeral:PAMLevel:LEVel{N}?
Description
For the PAM General global threshold, when the ABSolute method for PAM level definition is selected (see :MEASure:THReshold:PAM:GENeral:LMEThod), this command is used to specify the PAM level values.