:MEASure:THReshold:STHResholds

Command Syntax

:MEASure:THReshold:STHResholds  {OFF | GENeral | RFALl}

Query Syntax

:MEASure:THReshold:STHResholds?

Description

This command enables the display of level markers that can be dragged up or down to make adjustments. It has these options:

OFF
Interactive level markers are not displayed.
GENeral
For General measurements, when the ABSolute or HYSTeresis threshold methods are selected (see :MEASure:THReshold:GENeral:METHod), markers that show the threshold levels are displayed. Upper threshold, middle threshold, and lower threshold markers appear for the ABSolute threshold method. A single center threshold marker appears for the HYSTeresis threshold method.
For PAM3 General and PAM4 General measurements, when the HYSTeresis threshold method is selected (see :MEASure:THReshold:PAM:GENeral:METHod), markers that show the PAM threshold levels are displayed.
Also for PAM3 General and PAM4 General measurements, when the ABSolute level method is selected (see :MEASure:THReshold:PAM:GENeral:LMEThod), markers that show the PAM levels are displayed.
RFALl
For Rise/Fall time measurements, when the ABSolute threshold method is selected (see :MEASure:THReshold:RFALl:METHod), markers that show the upper and lower threshold levels are displayed.
For PAM3 Rise/Fall or PAM4 Rise/Fall time measurements, when the ABSolute level method is selected (see :MEASure:THReshold:PAM:RFALl:LMEThod), markers that show the PAM levels are displayed.