:MEASure:THReshold:GENeral:HYSTeresis
Command Syntax
:MEASure:THReshold:GENeral:HYSTeresis <plus_or_minus_value>
<plus_or_minus_value> is a double.
Query Syntax
:MEASure:THReshold:GENeral:HYSTeresis?
Description
When the :MEASure:THReshold:GENeral:METHod setting is HYSTeresis, this command sets the global threshold ±hysteresis value.
Use the :MEASure:THReshold:GENeral:MIDDle command to enter the center threshold level.
Example Command Sequence
:MEASure:THReshold:GENeral:METHod HYSTeresis :MEASure:THReshold:GENeral:HYSTeresis 125E-3 :MEASure:THReshold:GENeral:MIDDle 0E0