:MEASure:THReshold:PAM:RFALl:METHod

Command Syntax

:MEASure:THReshold:PAM{3|4}:RFALl:METHod  {P1090 | P2080 | PERCent | ABSolute}

Query Syntax

:MEASure:THReshold:PAM{3|4}:RFALl:METHod?

Description

For the PAM4 Rise/Fall global threshold, this command selects the threshold method:

P1090
Thresholds are set at the 10% and 90% locations between PAM levels.
P2080
Thresholds are set at the 20% and 80% locations between PAM levels.

To specify the method of determining the PAM levels, use the :MEASure:THReshold:PAM:RFALl:LMEThod command.