:MEASure:THReshold:GENeral:PUPPer

Command Syntax

:MEASure:THReshold:GENeral:PUPPer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Query Syntax

:MEASure:THReshold:GENeral:PUPPer?

Description

When the global threshold method is a custom PERCent between top and base (see :MEASure:THReshold:GENeral:METHod), the :MEASure:THReshold:GENeral:PUPPer command sets or queries the custom upper percent value.

Example Command Sequence

:MEASure:THReshold:GENeral:METHod PERCent
:MEASure:THReshold:GENeral:PUPPer 125E-3
:MEASure:THReshold:GENeral:PMIDdle 0E0
:MEASure:THReshold:GENeral:PLOWer -125E-3