Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MEASure:THReshold:PAM:RFALl:LMEThod

Threshold Definition Commands
  • :MEASure:TBASe:GENeral:BASE
  • :MEASure:TBASe:GENeral:METHod
  • :MEASure:TBASe:GENeral:TOP
  • :MEASure:TBASe:RFALl:BASE
  • :MEASure:TBASe:RFALl:METHod
  • :MEASure:TBASe:RFALl:TOP
  • :MEASure:THReshold:EREFerence
  • :MEASure:THReshold:GENeral:HYSTeresis
  • :MEASure:THReshold:GENeral:LOWer
  • :MEASure:THReshold:GENeral:METHod
  • :MEASure:THReshold:GENeral:MIDDle
  • :MEASure:THReshold:GENeral:PLOWer
  • :MEASure:THReshold:GENeral:PMIDdle
  • :MEASure:THReshold:GENeral:PUPPer
  • :MEASure:THReshold:GENeral:UPPer
  • :MEASure:THReshold:PAM:GENeral:HYSTeresis
  • :MEASure:THReshold:PAM:GENeral:LMEThod
  • :MEASure:THReshold:PAM:GENeral:METHod
  • :MEASure:THReshold:PAM:GENeral:PAMLevel:LEVel{N}
  • :MEASure:THReshold:PAM:GENeral:THResholds:EYE{N}
  • :MEASure:THReshold:PAM:RFALl:LMEThod
  • :MEASure:THReshold:PAM:RFALl:METHod
  • :MEASure:THReshold:PAM:RFALl:PAMLevel:LEVel{N}
  • :MEASure:THReshold:RFALl:LOWer
  • :MEASure:THReshold:RFALl:METHod
  • :MEASure:THReshold:RFALl:PLOWer
  • :MEASure:THReshold:RFALl:PUPPer
  • :MEASure:THReshold:RFALl:UPPer
  • :MEASure:THReshold:STHResholds

Command Syntax

:MEASure:THReshold:PAM{3|4}:RFALl:LMEThod  {AUTO | ABSolute}

Query Syntax

:MEASure:THReshold:PAM{3|4}:RFALl:LMEThod?

Description

For the PAM Rise/Fall global threshold, this command specifies the method used to determine the PAM levels:

AUTO
The PAM levels are automatically determined.
ABSolute
You specify the PAM levels using the :MEASure:THReshold:PAM:RFALl:PAMLevel:LEVel{N} command.