:MEASure:THReshold:GENeral:UPPer
Command Syntax
:MEASure:THReshold:GENeral:UPPer <amplitude>
<amplitude> is a double.
Query Syntax
:MEASure:THReshold:GENeral:UPPer?
Description
Sets or queries the General threshold's global upper threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :MEASure:THReshold:GENeral:PUPPer command.
Use the :MEASure:THReshold:GENeral:METHod command to set waveform threshold levels to standard percentages or custom definitions.
Use the :MEASure:THReshold:GENeral:MIDDle command to enter a middle threshold level. Use the :MEASure:THReshold:GENeral:LOWer command to enter a lower threshold level.
Example Command Sequence
:MEASure:THReshold:GENeral:METHod ABSolute :MEASure:THReshold:GENeral:UPPer 125E-3 :MEASure:THReshold:GENeral:MIDDle 0E0 :MEASure:THReshold:GENeral:LOWer -125E-3