:MEASure:THReshold:PAM:GENeral:THResholds:EYE{N}
Command Syntax
:MEASure:THReshold:PAM{3|4}:GENeral:THResholds:EYE{N} <amplitude>
Where {N} is the PAM eye threshold. For example, in PAM4, you can use EYE0 for the 0/1 threshold, EYE1 for the 1/2 threshold, or EYE2 for the 2/3 threshold.
<amplitude> is a double.
Query Syntax
:MEASure:THReshold:PAM{3|4}:GENeral:THResholds:EYE{N}?
Description
For the PAM General global threshold, when the HYSTeresis threshold method is selected (see :MEASure:THReshold:PAM:GENeral:METHod), this command is used to specify the PAM eye threshold values.