:MEASure:THReshold:PAM:GENeral:LMEThod

Command Syntax

:MEASure:THReshold:PAM{3|4}:GENeral:LMEThod  {AUTO | ABSolute}

Query Syntax

:MEASure:THReshold:PAM{3|4}:GENeral:LMEThod?

Description

For the PAM4 General global threshold, when the 50% of Levels threshold method is selected (see :MEASure:THReshold:PAM:GENeral:METHod), this command specifies the method used to determine the PAM levels:

AUTO
The PAM levels are automatically determined.
ABSolute
You specify the PAM levels using the :MEASure:THReshold:PAM:GENeral:PAMLevel:LEVel{N} command.