:WMEMory:THReshold:GENeral:AUTO
Command Syntax
:WMEMoryN:THReshold:GENeral:AUTO
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Description
When you select the ± Hysteresis threshold definition for the selected signal (see :WMEMory:THReshold:GENeral:METHod), you can send :WMEMory:THReshold:GENeral:AUTO to automatically set the Center Threshold (:WMEMory:THReshold:GENeral:MIDDle) to be halfway between Vmin and Vmax and the Hysteresis value (:WMEMory:THReshold:GENeral:HYSTeresis) to be ±0.05(Vmax - Vmin).