:WMEMory:THReshold:GENeral:PAM:PAMLevel:LEVel
Command Syntax
:WMEMoryN:THReshold:GENeral:PAM:PAMLevel:LEVel{0:3} <amplitude>
Where <amplitude> is a double.
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:THReshold:GENeral:PAM:PAMLevel:LEVel{0:3}?
Description
When specifying PAM general levels and you have selected the Absolute level method for the selected signal (see :WMEMory:TBASe:GENeral:METHod), this command sets or queries the PAM level values.
Use the :WMEMory:THReshold:GENeral:PAM:ASLevels command to automatically set the PAM levels.