:WMEMory:THReshold:RFALl:TOP

Command Syntax

:WMEMoryN:THReshold:RFALl:TOP amplitude

<amplitude> is a double.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:RFALl:TOP?

Description

For the indicated waveform memory, sets the Rise/Fall threshold's custom top-level setting. The top and base levels are used to locate a waveform's lower and upper threshold levels for the rise time, fall time, and slew rate measurements. Specify the level in volts or Watts depending on the waveform type. Use :WMEMory:THReshold:RFALl:BASE to set or query a custom base level.

Before this user-defined top level can be applied to measurements, use the :WMEMory:TBASe:RFALl:METHod command to select user-defined top-base definitions.

Example Command Sequence

:WMEMory2:THReshold:RFALl:TRACking OFF
:WMEMory2:TBASe:RFALl:METHod ABSolute
:WMEMory2:THReshold:RFALl:BASE -125E-3
:WMEMory2:THReshold:RFALl:TOP 125E-3