:WMEMory:THReshold:RFALl:PAM:PAMLevels:LEVel

Command Syntax

:WMEMoryN:THReshold:RFALl:PAM:PAMLevels:LEVel{0:3}  <amplitude>

Where <amplitude> is a double.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:RFALl:PAM:PAMLevels:LEVel{0:3}?

Description

When specifying PAM rise/fall levels and you have selected the Absolute level method for the selected signal (see :WMEMory:TBASe:RFALl:METHod), this command sets or queries the PAM level values.

Use the :WMEMory:THReshold:RFALl:PAM:ASLevels command to automatically set the PAM levels.