:WMEMory:THReshold:GENeral:PAM:THResholds:EYE

Command Syntax

:WMEMoryN:THReshold:GENeral:PAM:THResholds:EYE{0:2}  <amplitude>

Where <amplitude> is a double.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:GENeral:PAM:THResholds:EYE{0:2}?

Description

When specifying PAM general thresholds and you select the ± Hysteresis threshold definition for the selected signal (see :WMEMory:THReshold:GENeral:METHod), this command sets or queries the PAM eye threshold level. This value is used when making measurements.

Use the :WMEMory:THReshold:GENeral:HYSTeresis command to specify the amount of hysteresis.

Use the :WMEMory:THReshold:GENeral:PAM:ASTHresholds command to automatically set the PAM thresholds and hysteresis using a vertical histogram measurement.