:WMEMory:THReshold:GENeral:PLOWer

Command Syntax

:WMEMoryN:THReshold:GENeral:PLOWer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:GENeral:PLOWer?

Description

When the threshold method is a custom PERCent between top and base (see :WMEMory:THReshold:GENeral:METHod), the :WMEMory:THReshold:GENeral:PLOWer command sets or queries the custom lower percent value.

Example Command Sequence

:WMEMory2:THReshold:GENeral:TRACking OFF
:WMEMory2:THReshold:GENeral:METHod PERCent
:WMEMory2:THReshold:GENeral:PUPPer 125E-3
:WMEMory2:THReshold:GENeral:PMIDdle 0E0
:WMEMory2:THReshold:GENeral:PLOWer -125E-3