:WMEMory:THReshold:RFALl:PLOWer

Command Syntax

:WMEMoryN:THReshold:RFALl:PLOWer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:RFALl:PLOWer?

Description

When the threshold method is a custom PERCent between top and base (see :WMEMory:THReshold:RFALl:METHod), the :WMEMory:THReshold:RFALl:PLOWer command sets or queries the custom lower percent value.

Example Command Sequence

:WMEMory2:THReshold:RFALl:TRACking OFF
:WMEMory2:THReshold:RFALl:METHod PERCent
:WMEMory2:THReshold:RFALl:PUPPer 125E-3
:WMEMory2:THReshold:RFALl:PLOWer -125E-3