:WMEMory:THReshold:GENeral:BASE

Command Syntax

:WMEMoryN:THReshold:GENeral:BASE amplitude

<amplitude> is a double.

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:GENeral:BASE?

Description

For the indicated waveform memory, sets the General threshold's custom base-level. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels for measurements. Specify the level in volts or Watts depending on the waveform type. Use :WMEMory:THReshold:GENeral:TOP to set or query a custom top level.

Before this user-defined base level can be applied to measurements, use the :WMEMory:TBASe:GENeral:METHod command to select user-defined top-base definitions.

Example Command Sequence

:WMEMory2:THReshold:GENeral:TRACking OFF
:WMEMory2:TBASe:GENeral:METHod ABSolute
:WMEMory2:THReshold:GENeral:BASE -125E-3
:WMEMory2:THReshold:GENeral:TOP 125E-3