:WMEMory:THReshold:GENeral:TOP
Command Syntax
:WMEMoryN:THReshold:GENeral:TOP amplitude
<amplitude> is a double.
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:THReshold:GENeral:TOP?
Description
For the indicated waveform memory, sets the General threshold's custom top-level setting. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels for measurements. Specify the level in volts or Watts depending on the waveform type. Use :WMEMory:THReshold:GENeral:BASE to set or query a custom base level.
Before this user-defined top level can be applied to measurements, use the :WMEMory:TBASe:GENeral:METHod command to select user-defined top-base definitions.
Example Command Sequence
:WMEMory2:THReshold:GENeral:TRACking OFF :WMEMory2:TBASe:GENeral:METHod ABSolute :WMEMory2:THReshold:GENeral:BASE -125E-3 :WMEMory2:THReshold:GENeral:TOP 125E-3