:WMEMory:THReshold:GENeral:TRACking

Command Syntax

:WMEMoryN:THReshold:GENeral:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:GENeral:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the General threshold's global threshold definition or uses its own threshold definition.

The global threshold definition is set using the :MEASure:THReshold:GENeral commands (see Threshold Configuration Commands).

Example Command Sequence

:WMEMory2:THReshold:GENeral:TRACking OFF
:WMEMory2:THReshold:GENeral:METHod ABSolute
:WMEMory2:THReshold:GENeral:UPPer 125E-3
:WMEMory2:THReshold:GENeral:MIDDle 0E0
:WMEMory2:THReshold:GENeral:LOWer -125E-3