:WMEMory:THReshold:RFALl:BASE
Command Syntax
:WMEMoryN:THReshold:RFALl:BASE amplitude
<amplitude> is a double.
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:THReshold:RFALl:BASE?
Description
For the indicated waveform memory, sets the Rise/Fall threshold's custom base-level. The top and base levels are used to locate a waveform's lower and upper threshold levels for the rise time, fall time, and slew rate measurements. Specify the level in volts or Watts depending on the waveform type. Use :WMEMory:THReshold:RFALl:TOP to set or query a custom top level.
Before this user-defined base level can be applied to measurements, use the :WMEMory:TBASe:RFALl:METHod command to select user-defined top-base definitions.
Example Command Sequence
:WMEMory2:THReshold:RFALl:TRACking OFF :WMEMory2:TBASe:RFALl:METHod ABSolute :WMEMory2:THReshold:RFALl:BASE -125E-3 :WMEMory2:THReshold:RFALl:TOP 125E-3