:WMEMory:THReshold:RFALl:TRACking

Command Syntax

:WMEMoryN:THReshold:RFALl:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:THReshold:RFALl:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the Rise/Fall threshold's global threshold definition or uses its own threshold definition.

The global threshold definition is set using the :MEASure:THReshold:RFALl commands (see Threshold Configuration Commands).

Example Command Sequence

:WMEMory2:THReshold:RFALl:TRACking OFF
:WMEMory2:THReshold:RFALl:METHod ABSolute
:WMEMory2:THReshold:RFALl:UPPer 125E-3
:WMEMory2:THReshold:RFALl:LOWer -125E-3