:WMEMory:THReshold:RFALl:UPPer
Command Syntax
:WMEMoryN:THReshold:RFALl:UPPer amplitude
<amplitude> is a double.
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:THReshold:RFALl:UPPer?
Description
Sets the Rise/Fall threshold's upper threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :WMEMory:THReshold:RFALl:PUPPer command.
Use the :WMEMory:THReshold:RFALl:METHod command to set waveform threshold levels to standard percentages or custom definitions.
Use the :WMEMory:THReshold:RFALl:LOWer command to enter a lower threshold level.
Example Command Sequence
:WMEMory2:THReshold:RFALl:TRACking OFF :WMEMory2:THReshold:RFALl:METHod ABSolute :WMEMory2:THReshold:RFALl:UPPer 125E-3 :WMEMory2:THReshold:RFALl:LOWer -125E-3