:WMEMory:THReshold:GENeral:PAM:ASTHresholds
Command Syntax
:WMEMoryN:THReshold:GENeral:PAM:ASTHresholds
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Description
When specifying PAM general thresholds and you select the ± Hysteresis threshold definition for the selected signal (see :WMEMory:THReshold:GENeral:METHod), you can send this command to automatically set the PAM thresholds and hysteresis using a vertical histogram measurement.
The automatically determined PAM thresholds and hysteresis values can be adjusted using the :WMEMory:THReshold:GENeral:PAM:THResholds:EYE and :WMEMory:THReshold:GENeral:HYSTeresis commands.