:WMEMory:THReshold:GENeral:PAM:ASLevels
Command Syntax
:WMEMoryN:THReshold:GENeral:PAM:ASLevels
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Description
When specifying PAM general levels and you have selected the Absolute level method for the selected signal (see :WMEMory:TBASe:GENeral:METHod), you can send this command to automatically set the PAM levels.
The automatically determined PAM levels can be adjusted using the :WMEMory:THReshold:GENeral:PAM:PAMLevel:LEVel command.