:WMEMory:THReshold:GENeral:HYSTeresis
Command Syntax
:WMEMoryN:THReshold:GENeral:HYSTeresis plus_or_minus_value
<plus_or_minus_value> is a double.
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:THReshold:GENeral:HYSTeresis?
Description
When the :WMEMory:THReshold:GENeral:METHod setting is HYSTeresis, this command sets the user-defined ±hysteresis value for the waveform source.
Use the :WMEMory:THReshold:GENeral:MIDDle command to enter the center threshold value.
Example Command Sequence
:WMEMory2:THReshold:GENeral:TRACking OFF :WMEMory2:THReshold:GENeral:METHod HYSTeresis :WMEMory2:THReshold:GENeral:HYSTeresis 125E-3 :WMEMory2:THReshold:GENeral:MIDDle 0E0