FlexEye Analysis Commands
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Use the commands in the :FEYE subsystem to configure and run FlexEye Independent Eye Acquisition and Analysis. FlexEye can only be used with the HiSLIP VISA interface. FlexEye is not compatible with VXI-11, Telnet, Sockets, or GPIB.