:EMODules:AWGenerator:VADDress

AWG Instrument:
M8194/5/6A
M8199A/B
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
Licensed Feature:
F-AWG
Waveform type:
NRZ
PAM4/6/8
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:EMODules:AWGenerator{1:8}:VADDress "string"

Where {1:8} identifies slot number which is associated with an AWG instrument.

Where "string" is a the VISA address.

Query Syntax

:EMODules:AWGenerator{1:8}:VADDress?

Query Response

Returns the VISA address or an empty string if no address has been entered.

Description

Enter the SICL LAN interface address for an Arbitrary Waveform Generator (AWG) extended module. In the command, be sure to include the FlexDCA slot number where the AWG is installed. The following table lists several examples of different SICL LAN interface addresses. Use the :EMODules:SLOT:ADDRess command to select to use the SICL interface. To enter a SICL address instead, use the :EMODules:AWGenerator:SADDress command.

Example AWG VISA Address Strings
Using VISA Address
AWG hostname TCPIP0::WINDOWS-6ISM873::hislip0::INSTR
AWG IP address TCPIP0::10.113.25.62::hislip0::INSTR
localhost TCPIP0::localhost::hislip0::INSTR
Note: You can use localhost if FlexDCA is running on the AWG's AXIe Embedded Controller module.

Requires FlexDCA revision A.06.00 and above.

Example Command Sequence

:EMODules:AWGenerator6:VADDress "TCPIP0::WINDOWS-6ISM873::hislip0::INSTR"
:EMODules:SLOT6:ADDRess VISA