:SLOT:TRIGger:CRATe
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SLOT{1:8}:TRIGger:CRATe <rate>
Where the {1:8} specifier identifies a module slot.
<rate> is a double.
Query Syntax
:SLOT{1:8}:TRIGger:CRATe?
Description
When a Fractional clock ratio for pattern lock is selected using the :SLOT:TRIGger:DCDRatio:TYPE command, use the :SLOT:TRIGger:CRATe command to enter the actual clock rate. For example, for an 9.95328 GBd input signal you could enter:
:SLOT:TRIGger:CRATe 4.97664E9
Requires FlexDCA revision A.07.90 and above.
Example Command Sequence
:SLOT2:TRIGger:DCDRatio:TYPE FRACtional :SLOT2:TRIGger:CRATe 4.97664E9