:SLOT:TRIGger:DCDRatio:FRACtion
Instrument:
N109x
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:SLOT{1:8}:TRIGger:DCDRatio:FRACtion?
Where the {1:8} specifier identifies a module slot.
Query Response
Returns a float. For example, 1.60E+10.
Description
Returns the fractional clock ratio when a fractional clock is selected with the :SLOT:TRIGger:DCDRatio:TYPE command.
Requires FlexDCA revision A.07.90 and above.