:TDR:ADAPters:CONNector
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ADAPters:CONNector{1|2} {M350 | F350 | M292 | F292 | M240 | F240 | M185 | F185}
Query Syntax
:TDR:ADAPters:CONNector?
Description
Enters the RF adapter type that will be used on each of the two ECal module's connectors. Supported connector types include 1.85 mm, 2.4 mm, 2.92 mm, and 3.5 mm (both male and female).
| Connector Type | Command Argument | |
|---|---|---|
| Male | Female | |
| 3.5 mm | M350 | F350 |
| 2.92 mm | M292 | F292 |
| 2.4 mm | M240 | F240 |
| 1.85 mm | M185 | F185 |
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:ADAPters:CONNector2 M185