:TDR:CALibration:DUT:ECAL:ADAPters:D
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:ECAL:ADAPters:D <adapter name>
The <adapter name> argument is a string.
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Syntax
:TDR:CALibration:DUTN:ECAL:ADAPters:D?
Description
For an ECal-based TDR calibration, specifies a user-defined adapter that is used to connect the TDR head to Port D on the ECal module. The <adapter name> argument is the name that you created using the :TDR:ADAPters:NAME command for the Adapter wizard. The Adapter wizard (:TDR:ADAPters:STARt command) specifies an adapter's name, connectors, and delay. The command query returns the currently assigned adapter for Port A on the ECal module. If no adapter is assigned, None is returned.
Example Command Sequence
:TDR:ADAPters:STARt // Specify first ECal adapter :TDR:ADAPters:SDONe? :TDR:ADAPters:NAME "1.85m 2.9f Adapter" :TDR:ADAPters:CONTinue … :TDR:ADAPters:STARt // Specify second ECal adapter :TDR:ADAPters:SDONe? :TDR:ADAPters:NAME "1.85m 2.92m Adapter" :TDR:ADAPters:CONTinue … :TDR:CALibration:DUT1:ECAL:ADAPters:A "1.85m 2.9f Adapter" // ECal module Port A adapter :TDR:CALibration:DUT1:ECAL:ADAPters:D "1.85m 2.92m Adapter" // ECal module Port D adapter … … :TDR:CALibration:DUT1:STARt
Requires FlexDCA revision A.07.90 and above.