:TDR:CALibration:DUT:ECAL:STATus:REASon
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:CALibration:DUTN:ECAL:STATus:REASon?
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Description
Returns a message about the ECal module. For a valid ECal module, an empty string is returned. For an invalid or missing ECal module, an informational message is returned such as these examples:
"No ECal modules detected." "Currently selected ECal module is not supported."
Use the parent :TDR:CALibration:DUT:ECal:STATus query, to return the status of the ECal module.
Requires FlexDCA revision A.04.00 and above.