:TDR:CALibration:DUT:ECAL:MODule

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter

Command Syntax

:TDR:CALibration:DUTN:ECAL:MODule "ECal (<model number>) S/N <serial number>

Where N indicates one of 16 possible DUT setups. For example, :DUT4.

Query Syntax

:TDR:CALibration:DUTN:ECAL:MODule?

Description

Selects a specific ECal module for an ECal based TDR calibration when multiple ECal modules are connected to the N1000A. If a single ECal module is connected to the N1000A, the ECal module is automatically detected and selected. The parameter string specifying the module must include the ECal module's model and serial numbers. The string is not case sensitive, but spaces, parenthesis, leading zeros in the serial number are all required. The following example strings are valid:

"ECal (N4694-60002) S/N 08485"
"ecal (N4694-60002) s/n 08485"

However, these string are not valid:

"ECal (N4694-60002) S/N 8485"    //  missing leading S/N zero
"ECal (N4694-60002) 08485"    //  missing S/N characters
"ECal(N4694-60002) S/N 08485"    //  missing space

Recommended ECal Modules

  • N4696D-0DC- F0F, M0M or M0F (18 GHz)
  • N4694D-0DC- F0F, M0M or M0F (67 GHz)
  • N4694A-HMM, HFF or HMF
  • N4693D-0DC- F0F, M0M or M0F (50 GHz)
  • N4692D-0DC- F0F, M0M or M0F (40 GHz)
  • N4691D-0DC- F0F, M0M or M0F (26.5 GHz)
  • N4433D-0DC- F0F, M0M or M0F (26.5 GHz)
  • N755xA-3FF (Both 3.5 mm connectors are female on module)
  • N755xA-3MF (1 female and 1 male connector on module, both 3.5 mm)
  • N755xA-3MM (Both 3.5 mm connectors are male on module)

Requires FlexDCA revision A.04.00 and above.