:TDR:ADAPters:SCHannel
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ADAPters:SCHannel CHANnel{1:8}{A|B|C|D}
Where the {1:8}{A|B|C|D} specifier identifies a channel.
Query Syntax
:TDR:ADAPters:SCHannel?
Description
When the Add New Adapter wizard is configured for measuring the adapter's delay value rather manual entering it, use this command to select the channel (TDR head) for making the measurement. To select that the delay value is to be measured, use the :TDR:ADAPters:DSPec command.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:ADAPters:SCHannel CHANnel2C