:TDR:ADAPters:DELay
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ADAPters:DELay <delay>
<delay> is a double.
Query Syntax
:TDR:ADAPters:DELay?
Description
Enters the adapter's delay in seconds. This command is used when the Add New Adapter wizard is configured for manual entry of the delay value rather than measuring the delay. Use the :TDR:ADAPters:DSPec command to select the delay entry method used.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:ADAPters:DELay 3.62E-04