:TDR:ADAPters:NAME
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ADAPters:NAME <string>
Query Syntax
:TDR:ADAPters:NAME?
Description
Adds an identifying name to an adapter that is being added in the Add New Adapter wizard. The name is a string limited to 20 characters or less. If the adapter name already exists, use the :TDR:ADAPters:OVERwrite command to overwrite the current adapter. To start the wizard, use the :TDR:ADAPters:STARt command. After defining your adapter, use this name to assign the adapter to the ECal module using the :TDR:CALibration:DUT:ECAL:ADAPters:A or :TDR:CALibration:DUT:ECAL:ADAPters:B commands.
If you need to delete an adapter definition, delete the definition file.
Requires FlexDCA revision A.04.00 and above.