:TDR:ADAPters:OVERwrite
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ADAPters:OVERwrite
Description
This command is used when the Add New Adapter wizard step for naming a new adapter is displayed and the adapter name already exists. Use the :TDR:ADAPters:OVERwrite command to overwrite the current adapter. This is equivalent to clicking the Overwrite button that is shown in the wizard.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:ADAPters:OVERwrite