:TDR:ADAPters:SDONe?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:ADAPters:SDONe?
Description
During the Add New Adapter wizard, sets an interupt to indicate the next wizard step is viewed. Send this query after the :TDR:ADAPters:STARt and :TDR:ADAPters:CONTinue commands as shown in the example for the :TDR:ADAPters:STARt command.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:ADAPters:SDONe?