:TDR:ADAPters:STARt
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ADAPters:STARt
Description
For an ECal-based TDR calibration, starts the Add New Adapter wizard, which is required to specify an adapter that connects the ECal module to the TDR head. This wizard measures (or allows you to manually enter) the delay introduced by the adapter. Use the :TDR:ADAPters:DSPec command to specify if the adapter's delay value is manually entered or measured. To assign the adapter to either the ECal module's A or B port, use the :TDR:CALibration:DUT:ECAL:ADAPters:A and :TDR:CALibration:DUT:ECAL:ADAPters:Bcommands.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:TDR:ADAPters:STARt :TDR:ADAPters:SDONe? // View "Set Adapter Name" step. :TDR:ADAPters:NAME "Adapter C" // Name adapter. :TDR:ADAPters:CONTinue // "Click" Next. :TDR:ADAPters:SDONe? // View "Describe Adapter" step. :TDR:ADAPters:CONNector1 F240 // Type of adapter connector. :TDR:ADAPters:CONNector2 F240 :TDR:ADAPters:DSPec MDELay // Select to measure the delay. :TDR:ADAPters:CONTinue // "Click" Next. :TDR:ADAPters:SDONe? // View "Select Channel" step. :TDR:ADAPters:SCHAnnel CHAN1A // Select the channel. :TDR:ADAPters:CONTinue // "Click" Next. :TDR:ADAPters:SDONe? // Vew "Attach Adapter" instruction. :TDR:ADAPters:CONTinue // "Click" Next. :TDR:ADAPters:SDONe? // Vew "Remove Adapter" instruction. :TDR:ADAPters:CONTinue // "Click" Next. :TDR:ADAPters:SDONe? // Vew "Verify Delay" instruction. :TDR:ADAPters:CONTinue // "Click" Next. :TDR:ADAPters:SDONe? // Vew "Completed" notice. :TDR:ADAPters:CONTinue // "Click" Done. *OPC?