:TDR:CALibration:DUT:ECAL:CHAR
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:ECAL:CHAR <characterization>
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Where <characterization> is a string.
Query Syntax
:TDR:CALibration:DUTN:ECAL:CHAR?
Query Response
FACTOR
Description
Selects the base characterization of the specified eCal module. This command is equivalent to using the Characterization drop-down list when specifying an eCal based TDR calibration. Currently, all eCal modules supported by TDR/TDT mode have only one available characterization which is "Factory". This is indicated in the query response, which is always "FACTOR".
Requires FlexDCA revision A.04.00 and above.