:TDR:CALibration:DUT:ECAL:STATus?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:CALibration:DUTN:ECAL:STATus?
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Query Response
{CORR | INV}
Description
Returns the status of the ECal module for an ECal-based calibration. The status can be correct (CORR) or invalid (INV). Use the :REASon child query to return a message about the module.
Requires FlexDCA revision A.04.00 and above.