:WMEMory:CWINdow
Command Syntax
:WMEMory{1:8}:CWINdow TIMe{1}
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:CWINdow?
Description
The :WMEMory{1:8}:CWINdow command allows you to assign a waveform memory waveform to a Waveform content window.
As of this release, there is only one Waveform content window, so you will not need to use this command.
In future revisions, the :WMEMory{1:8}:CWINdow command will select a content window in which to display a waveform memory waveform. In FlexDCA, four different types of content windows exist: Waveform (TIMe1), Group Delay (GDELay), Magnitude (MAGNitude), and Phase (PHASe). Each type varies by its type of X- and Y-axis units. Any given waveform is only compatible with one of these four content window types. Therefore, FlexDCA automatically assigns waveforms to the proper type of content window, such as Waveform or Phase. Waveforms can not be assigned to a different type of content window. For example, a Waveform waveform can not be moved to or shown in a Magnitude content window.
| Argument | Displayed Waveform Content Window |
Number of Available Windows |
Scale Units | |
|---|---|---|---|---|
| Programmatically | Via Front Panel |
|||
| TIMe1 | Waveform | 1 | 1 | Y-Axis: Volts or Watts (linear scale) X-Axis: seconds |
Requires FlexDCA revision A.03.00 and above.