:WMEMory:DSTatus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Query Syntax
:WMEMory{1:8}:DSTatus?
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Response
{CORR | INV}
Description
Returns the status of the specified waveform memory. Up to eight memories are available. To query the reason for the current state of the memory, use the :WMEMory:DSTatus:REASon? query. The following responses can be returned:
CORR- The memory location contains waveform data. To clear memory, use the
:WMEMory:CLEarcommand. INV- The memory location does not contain waveform data.
Requires FlexDCA revision A.05.70 and above.